LTE FDD

Full-filled Config

For Real-Time capability.

Full-filled Config sets the channels with fully filled UL-SCH configuration. This button is shown when an uplink carrier is selected in the vertical tabs of the upper pane.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform:RTIMe:CCARrier<n>:ULINk:CONFig:FFILled <string>

SCPI Example

:RAD:LTEF:WAV:RTIM:CCAR:ULIN:CONF:FFIL "SystemBandwidth:B5M,Modulation:QPSK"

Notes

Set only (Immediate Action)

<string>: "name:value,name:value,…"

State Saved

No

Preset

Refer to the element definition of the data part below.

Range

Refer to the element definition of the data part below.

Initial S/W Revision

A.14.00

Element definition of the data part. The preset value is basically the same as the default value of each setting definition.

Settings

Symbols in the data part

Values in the data part

Preset values

System Bandwidth

SystemBandwidth

B1M4|B3M|B5M|B10M|B15M|B20M

B10M

Modulation

Modulation

QPSK|QAM16|QAM64|QAM256

QPSK

System Bandwidth

Sets System Bandwidth for full filled configuration.

SCPI Command

–

SCPI Example

–

Notes

No SCPI, GUI only, Set and Query

State Saved

No

Preset

10 MHz (50RB)

Range

1.4 MHz (6RB) | 3 MHz (15RB) | 5 MHz (25RB) | 10 MHz (50RB) | 15 MHz (75RB) | 20 MHz (100RB)

Initial S/W Revision

A.14.00

Modulation

Sets Modulation type for full filled configuration.

SCPI Command

–

SCPI Example

–

Notes

No SCPI, GUI only, Set and Query

State Saved

No

Preset

QPSK

Range

QPSK | 16QAM | 64QAM | 256QAM

Initial S/W Revision

A.14.00

Carrier Uplink ARB

Welcome to LTE FDD